2017-01-03 11:15 PM
If i do not disconnect the STM32 Boards serial USB connection to the PC Windows 7 I gets an BSOD on shut down.
2017-01-04 12:06 AM
Problemsignatur:
Problemereignisname: BlueScreen Betriebsystemversion: 6.1.7601.2.1.0.256.48 Gebietsschema-ID: 2055Zusatzinformationen zum Problem:
BCCode: 9f BCP1: 0000000000000003 BCP2: FFFFFA8013BAE060 BCP3: FFFFF80000B9A3D8 BCP4: FFFFFA801401D640 OS Version: 6_1_7601 Service Pack: 1_0 Product: 256_1Dateien, die bei der Beschreibung des Problems hilfreich sind:
C:\Windows\Minidump\010417-6942-01.dmp C:\Users\widmert\AppData\Local\Temp\WER-18517-0.sysdata.xmlLesen Sie unsere Datenschutzbestimmungen online:
Wenn die Onlinedatenschutzbestimmungen nicht verfügbar sind, lesen Sie unsere Datenschutzbestimmungen offline:
C:\windows\system32\de-DE\erofflps.txt2017-01-04 01:15 AM
BugCheck 9F, {3, fffffa8013bae060, fffff80000b9a3d8, fffffa801401d640}
*** ERROR: Module load completed but symbols could not be loaded for iusb3hub.sysProbably caused by : iusb3hub.sys2017-01-04 01:23 AM
It is not usb hub spesific. I tried it with several USB-Hubs all the same.
All ports gets disabled only the USB port of the STM32 Serial-USB Connect remains active.
2017-01-04 03:12 AM
Update to latest driver version of the On-board USB Host Controller didn't help.