cancel
Showing results for 
Search instead for 
Did you mean: 

USB MSC Implementation on Nucleo-F439ZI with FatFs Support

ajith1
Associate II

 

Hi STM32 Team,

I am working on implementing a USB Mass Storage Class (MSC) application on the Nucleo-F439ZI development board. My objective is to use the Fat Fs file system to read/write data from/to a USB flash drive.

I need example code for that. For example I need to create a text document.

Kindly do needful,

 

Thanks and Regards,

A. Ajith Kumar

1 REPLY 1
FBL
ST Employee

Hi @ajith1 

Check the following example

STM32CubeF4/Projects/STM32F429ZI-Nucleo/Applications/FatFs/FatFs_USBDisk at master · STMicroelectronics/STM32CubeF4

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!