2024-07-25 04:35 PM
Hi all
I would like to know if I can use the CDC example to transmit and receive data from the windows host without redirecting it to UART
Solved! Go to Solution.
2024-07-25 06:11 PM
Yes, that is what USB CDC does. The interface is presented as a serial port, but all communication occurs over USB packets, not UART signals. You can select baud rate and other parameters but they aren't actually used.
2024-07-25 06:11 PM
Yes, that is what USB CDC does. The interface is presented as a serial port, but all communication occurs over USB packets, not UART signals. You can select baud rate and other parameters but they aren't actually used.