cancel
Showing results for 
Search instead for 
Did you mean: 

USB CDC Example - using the ode to receive and transmit data from USB interface

Rajam
Associate II

Hi all 

I would like to know if I can use the CDC example to transmit and receive data from the windows host without redirecting it to UART

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Yes, that is what USB CDC does. The interface is presented as a serial port, but all communication occurs over USB packets, not UART signals. You can select baud rate and other parameters but they aren't actually used.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Guru

Yes, that is what USB CDC does. The interface is presented as a serial port, but all communication occurs over USB packets, not UART signals. You can select baud rate and other parameters but they aren't actually used.

If you feel a post has answered your question, please click "Accept as Solution".