2017-04-11 3:39 AM
Hi all
I'm working on a STM32F303CC very simple board(just µC IMU and USB). I need to use a USB Virtual COM (CDC) for a MtoM data transfer with a Windows PC I set up BSP with STMCubeMx and compiling/debuging with Keil V5 with an STlink V2 in SWD mode board and microcontrolers are powered by USB all look's working great when I make a hard reset (just fresh power up) but if I try to make a soft reset like when entering in debug despite Virtual Com Port is well enumerated on windows side it could not open com port and no Usb transmit can be done on target side becase of Usb Device descriptor not defined in Usb Midle ware does anyone faced the same issue or somthing similare ? I tried to use USBLyser to see what's wrong but I must admit I've not seen something particular when doing soft reset thank's for any helpSolved! Go to Solution.
2017-04-20 10:18 AM
YES !!!!!
I finaly found a way to force the USB master to forget the device and do the enumeration procedure completly
i'm calling this :/*pull down the USB RP pin to let think of master that device have been disconnect and force new device identification when calling MX_USB_DEVICE_Init() */
void USB_DEVICE_MasterHardReset(void)
{ GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,0); HAL_Delay(1000);}just before MX_USB_DEVICE_Init(); call I think delai could be reduced a lot (I'm not sure it is mandatory even) but I was so happy to to say it that I did not take time to ajust that yet
I hope it will help. I'm so surprised nobody encounter this before.
2017-04-11 7:57 AM
Hi,
Try
i
ncrease the heap and stack size and refer to the CDC example from STM32CubeF3 firmware package this will help you on your porject.
Imen
2017-04-20 6:27 AM
hi Imen thank's for your fast reply (and sory for my slow one )
unfortunatly I already tried to increase Heap and Stack
Stack_Size EQU 0x4000
Heap_Size EQU 0x2000
I based my CDC framework calls on the Cube Example I realy think there is something different between debug reset and power on
when I start a debug session the hUsbDeviceFS.pClassData struct stay null and CDC_Transmit_FS return immediatly
I've folowed calls to determine where pClassData would be initialised and I didnt realy figured what causes this but one again after a power on all works perfectly
after few more test I think problem comes because when soft reseting the Device on USB window master side is not unmount/reset ... I tried to call USBD_Stop() and USBD_DeInit() before main MX_USB_DEVICE_Init() call but as the hUsbDeviceFS has not been properly initialised it dead lock by calling null function pointers ( pdev->pClass->DeInit() for the first one)
I tried also to set CNTR register to force reset before init
/* disable all interrupts and force USB reset */
USB->CNTR = USB_CNTR_FRES; /* clear interrupt status register */ USB->ISTR = 0U; /* switch-off device */ USB->CNTR = (USB_CNTR_FRES | USB_CNTR_PDWN);but it did nothing too
the objective is to force the master to forget reseted device and be aware to a new device connect procedure
I continue to play in device register trying to force it to reset but if there is a good way to do it I will be gratefull !!
thank's for any help
2017-04-20 10:18 AM
YES !!!!!
I finaly found a way to force the USB master to forget the device and do the enumeration procedure completly
i'm calling this :/*pull down the USB RP pin to let think of master that device have been disconnect and force new device identification when calling MX_USB_DEVICE_Init() */
void USB_DEVICE_MasterHardReset(void)
{ GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,0); HAL_Delay(1000);}just before MX_USB_DEVICE_Init(); call I think delai could be reduced a lot (I'm not sure it is mandatory even) but I was so happy to to say it that I did not take time to ajust that yet
I hope it will help. I'm so surprised nobody encounter this before.
2025-01-03 5:19 AM - edited 2025-01-03 5:37 AM
Thank you so much @o gaste! I have been fighting with the same issue for hours. Your solution worked perfectly!
Here is a FreeRTOS safe version:
```
void USB_Reset(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,0);
#ifdef osCMSIS
// FreeRTOS is detected
osDelay(10);
#else
HAL_Delay(10);
#endif
}
```