Skip to main content
kdeganck9
Associate
October 22, 2009
Question

usart3 remapping

  • October 22, 2009
  • 5 replies
  • 1239 views
Posted on October 22, 2009 at 10:28

usart3 remapping

    This topic has been closed for replies.

    5 replies

    kdeganck9
    kdeganck9Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:26

    I do not succeed in 'half' remapping the USART3 on a STM32F103RB device (64LQFP, 128K Flash/20K RAM)

    The software works when port 3 in not remapped (with I2C2 clock disabled) and uses the same code as for port 1 and 2.

    The pins PC10 and PC11 can be toggled when used as push pull output.

    Has anyone experienced a similar problem or can just advice me in what to do next ?

    Thanks in advance.

    The code below shows the only difference between remap or not by means of the definition of 'USART3_PartialRemap'.

    #ifdef USART3_PartialRemap

    /* Configure USART3 Rx (PC.11) as input floating */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOC, &GPIO_InitStructure);

    /* Configure USART3 Tx (PC.10) as alternate function push-pull */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init(GPIOC, &GPIO_InitStructure);

    GPIO_PinRemapConfig( GPIO_PartialRemap_USART3, ENABLE );

    #else

    /* Configure USART3 Rx (PB.11) as input floating */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    /* Configure USART2 Tx (PB.10) as alternate function push-pull */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    #endif

    RCC_APB1PeriphClockCmd( RCC_APB1Periph_USART3, ENABLE);

    kdeganck9
    kdeganck9Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:26

    Dear Clive,

    Thanks for your response.

    I tried on a 'RET6' device too and I have the same problem.

    The GPIO clocks are enabled, otherwise I would be able to toggle the pins via JTAG.

    I also tried the remap statement before and after.

    But in the next coming days I'll try some other things you propose.

    regards,

    Koen

    clive2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:26

    I'm using USART3 in partial remap mode, also using flow control on a STM32F103RET6 (64LQFP, 512K/64K). Initialization code is similar to yours, I have the remap statement before the GPIO init. I have a GSM modem attached, works fine.

    Would look at GPIO-C clock. For the flow control to work you have to park the CAN controller off the RTS/CTS pins, otherwise it interferes with the operation (see errata)

    Finally after configuring the pins, enable the clock, then the USART

    ..

    else if (Uart->Port == USART3)

    {

    /* Enable USART3 Clock */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

    }

    USART_Cmd(Uart->Port, ENABLE); /* Enable the USART */

    ..

    What is the failure mode? Do you not see data on the Tx pin? Is the USART taking data and do you see the registers/status reflect changing internal state?

    -Clive

    kdeganck9
    kdeganck9Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:26

    Domen,

    Thank you very much.

    Now it works.

    domen2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:26

    AFIO clock?