2018-02-11 6:00 AM
Hello everyone. I have encountered problem with USART1 on STM32F446RE. It seems it doesn't work for me. I have used multiple times USART2 and it works as it should, but USART1 with same configurations just refuse to work. What could be the problem?
I use STM32CubeMX v4.24.0.
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart2;void SystemClock_Config(void);
static void MX_GPIO_Init(void);static void MX_USART1_UART_Init(void);static void MX_USART2_UART_Init(void);int main(void)
{ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); while (1) { HAL_UART_Transmit_IT(&huart1, (uint8_t *)'Hello with USART1\r\n', strlen('Hello with USART1\r\n')); HAL_Delay(1000); HAL_UART_Transmit_IT(&huart2, (uint8_t *)'Hello with USART2\r\n', strlen('Hello with USART2\r\n'));}
}
static void MX_USART1_UART_Init(void)
{huart1.Instance = USART1;
huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
static void MX_USART2_UART_Init(void){huart2.Instance = USART2;
huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
Solved! Go to Solution.
2018-02-11 9:19 AM
Not sure I understand the question.
The ST-LINK VCP is connected to PA2/PA3 (USART2), you can't create imaginary connectivity. Review schematic.
2018-02-11 6:04 AM
You should be looking at the MSP code that enables the clocks and pins.
stm32f4xx_hal_msp.c ?
2018-02-11 7:41 AM
,
,
This is the code of ,
stm32f4xx_hal_msp.c , . Maybe you have some insights what could be wrong?
♯ include 'stm32f4xx_hal.h'
extern void _Error_Handler(char *, int),
void HAL_MspInit(void)
,
{, , ,HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4),
,
, , ,HAL_NVIC_SetPriority(MemoryManagement_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(BusFault_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(UsageFault_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(SVCall_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(DebugMonitor_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(PendSV_IRQn, 0, 0),,
, , ,HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0),,
}void HAL_UART_MspInit(UART_HandleTypeDef* huart)
,
{, , ,GPIO_InitTypeDef GPIO_InitStruct,
,
, , ,if(huart->,Instance==USART1),
, , ,{,
, , , , , ,__HAL_RCC_USART1_CLK_ENABLE(),,
,
, , , , , ,/**USART1 GPIO Configuration,
, , , , , ,PA9 ------>, USART1_TX,
, , , , , ,PA10 ------>, USART1_RX,
, , , , , ,*/,
, , , , , ,GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10,,
, , , , , ,GPIO_InitStruct.Mode = GPIO_MODE_AF_PP,,
, , , , , ,GPIO_InitStruct.Pull = GPIO_PULLUP,,
, , , , , ,GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH,,
, , , , , ,GPIO_InitStruct.Alternate = GPIO_AF7_USART1,,
, , , , , ,HAL_GPIO_Init(GPIOA, &,GPIO_InitStruct),,
, , , , , ,HAL_NVIC_SetPriority(USART1_IRQn, 5, 0),,
, , , , , ,HAL_NVIC_EnableIRQ(USART1_IRQn),,
, , ,},
, , ,else if(huart->,Instance==USART2),
, , ,{,
, , , , , ,__HAL_RCC_USART2_CLK_ENABLE(),,
,
, , , , , ,/**USART2 GPIO Configuration,
, , , , , ,PA2 ------>, USART2_TX,
, , , , , ,PA3 ------>, USART2_RX,
, , , , , ,*/,
, , , , , ,GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3,,
, , , , , ,GPIO_InitStruct.Mode = GPIO_MODE_AF_PP,,
, , , , , ,GPIO_InitStruct.Pull = GPIO_PULLUP,,
, , , , , ,GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH,,
, , , , , ,GPIO_InitStruct.Alternate = GPIO_AF7_USART2,,
, , , , , ,HAL_GPIO_Init(GPIOA, &,GPIO_InitStruct),,
, , , , , ,HAL_NVIC_SetPriority(USART2_IRQn, 0, 0),,
, , , , , ,HAL_NVIC_EnableIRQ(USART2_IRQn),,
, , ,}}
void HAL_UART_MspDeInit(UART_HandleTypeDef* huart)
,
{, , ,if(huart->,Instance==USART1)
,
, , ,{,
, , , , , ,__HAL_RCC_USART1_CLK_DISABLE(),,
,
, , , , , ,/**USART1 GPIO Configuration,
, , , , , ,PA9 ------>, USART1_TX,
, , , , , ,PA10 ------>, USART1_RX,
, , , , , ,*/,
, , , , , ,HAL_GPIO_DeInit(GPIOA, GPIO_PIN_9|GPIO_PIN_10),, , , , , ,HAL_NVIC_DisableIRQ(USART1_IRQn),
,
, , ,},
, , ,else if(huart->,Instance==USART2),
, , ,{,
, , , , , ,__HAL_RCC_USART2_CLK_DISABLE(),,
,
, , , , , ,/**USART2 GPIO Configuration,
, , , , , ,PA2 ------>, USART2_TX,
, , , , , ,PA3 ------>, USART2_RX,
, , , , , ,*/,
, , , , , ,HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2|GPIO_PIN_3),,
, , , , , ,HAL_NVIC_DisableIRQ(USART2_IRQn),,
, , ,}}
2018-02-11 7:53 AM
Would probably use following for a local/auto variable to guarantee clean initialization
GPIO_InitTypeDef GPIO_InitStruct = {0};
And add
__GPIOA_CLK_ENABLE();
Is this a custom board, or a NUCLEO/DISCO ?
How are things wired up?
2018-02-11 8:17 AM
This is STM32F446RE Nucelo board, i don't have anything wired since i use only USART to output information through serial.
I have added the lines you but it doesn't seem to change anything. Maybe it can only communicate through GPIO, not serial.
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{GPIO_InitTypeDef GPIO_InitStruct = {0};
if(huart->Instance==USART1) { /* USER CODE BEGIN USART1_MspInit 0 */ __GPIOA_CLK_ENABLE(); /* USER CODE END USART1_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART1_CLK_ENABLE();.......
2018-02-11 8:42 AM
PA9/PA10 should get to the Arduino header
2018-02-11 8:51 AM
So this means, i can only transfer through serial USART2 and USART1 only through GPIO pins?
2018-02-11 9:18 AM
By default, on Nuc 64 boards, the USART2 is connected to STLINK.
2018-02-11 9:19 AM
Not sure I understand the question.
The ST-LINK VCP is connected to PA2/PA3 (USART2), you can't create imaginary connectivity. Review schematic.
2018-02-11 9:20 AM
see page 27 of UM1724