2021-08-24 06:51 AM
I am using STM32F746G discovery board.
~~~
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
HAL_UART_Receive_IT (&huart6, Rx_buff, USART_RX_BUFFER_SIZE);
HAL_Delay(500);
HAL_UART_Transmit(&huart6, &Rx_buff, USART_RX_BUFFER_SIZE, 1000);
}
~~~
This is the way i am using USART6, TX and RX.
here my doubt is, i fixed my USART_RX_BUFFER_SIZE =10.
I send 10 bytes data via serial terminal(hercules), in this case my usart transmit also works with same 10 bytes data.
But i send 9 bytes data means, the uart transmit is not transmit the 9 bytes data.
my requirement is,
how much amount of bytes received via UART_Receive(); , that amount of bytes, send via UART_Transmit();
Thanks
Manikandan D
Solved! Go to Solution.
2021-08-25 10:04 PM
Now my doubt is clear. Inside ISR function they are typecasting the Rx_buff.
like,
HAL_DMA_Start_IT(huart->hdmarx, (uint32_t)&huart->Instance->RDR, (uint32_t)huart->pRxBuffPtr, Size)
Because Function declaration of HAL_DMA_Start_IT is,
HAL_StatusTypeDef HAL_DMA_Start_IT(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength);
Thanks for your replies