2015-05-05 12:24 AM
Hello all,
I am novice to STM family. Here is the code which I have written for USART but not working .void UsartInit(void)
{ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_Pin_2, GPIO_AF_USART2); GPIO_PinAFConfig(GPIOA, GPIO_Pin_3, GPIO_AF_USART2); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength=USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity= USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl=USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE); }int main(void)
{ char ch='A'; UsartInit(); while(1) { while (USART_GetFlagStatus(USART2, USART_FLAG_TXE) != SET); USART_SendData(USART2, ch); Delay(0x3FFFFF); } }I have no idea what I am missing here ...
I need help to rectify the error. I have simply connected PA2 to the receiver of MAX232. Still I am not getting data on minicom, #uart-+-discovery-board2015-05-05 12:47 AM
Try GPIO_PinSourceX as argument of GPIO_PinAFConfig instead of GPIO_PinX.
2015-05-05 02:35 AM
thank u so much :)