cancel
Showing results for 
Search instead for 
Did you mean: 

USART not working while enabling Watch dog timer(WWDG) in stm32f105RB.

sG.12
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

I don't believe the two are connected, perhaps expand on the detail, with minimal code example, so the issue might be reviewed or replicated. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
 
#include "main.h"
 
#include "stm32f1xx_hal.h"
CAN_HandleTypeDef hcan1;
WWDG_HandleTypeDef hwwdg;
 
UART_HandleTypeDef huart1;
 
static CanTxMsgTypeDef myTxMessage;
 
static CanRxMsgTypeDef myRxMessage;
 
static CAN_FilterConfTypeDef myFilter;
 
 
 uint32_t j;
uint8_t *Rcbuff;
 
   uint8_t id,dlc,data[8];
 
void SystemClock_Config(void);
 
static void MX_GPIO_Init(void);
 
static void MX_WWDG_Init(void);
 
static void MX_CAN1_Init(void);
 
static void MX_USART1_UART_Init(void);
 
int main(void)
 
{
 
 
 
 HAL_Init();
 
 
 
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 
 MX_WWDG_Init();
 
 MX_CAN1_Init();
 
   MX_USART1_UART_Init();
 
   myFilter.FilterNumber          = 0;
 
   myFilter.FilterMode            = CAN_FILTERMODE_IDMASK;
 
   myFilter.FilterScale           = CAN_FILTERSCALE_32BIT;
 
   myFilter.FilterIdHigh          = 0x0000;
 
   myFilter.FilterIdLow           = 0x0000;
 
   myFilter.FilterMaskIdHigh      = 0x0000;
 
   myFilter.FilterMaskIdLow       = 0x0000;
 
   myFilter.FilterFIFOAssignment  = 0;
 
   myFilter.FilterActivation      = ENABLE;
 
 
   HAL_CAN_ConfigFilter(&hcan1,&myFilter);
 
   hcan1.pTxMsg = &myTxMessage;
 
   myTxMessage.DLC = 8;
 
 myTxMessage.StdId = 0x123;
 
 myTxMessage.IDE = CAN_ID_STD;
 
   myTxMessage.RTR=CAN_RTR_DATA;
 
   myTxMessage.Data[0]=0xAB;
 
 myTxMessage.Data[1]=0xCD;
 
 myTxMessage.Data[2]=0xEF;
 
 myTxMessage.Data[3]=0xAA;
 
 myTxMessage.Data[4]=0xBB;
 
   myTxMessage.Data[5]=0xCC;
 
   myTxMessage.Data[6]=0xDD;
 
   myTxMessage.Data[7]=0xEE; 
 
   //HAL_CAN_Transmit_IT(&hcan1);
 
      HAL_Delay(1000);
 
 
 
 while (1)
 
 {
 
 
   Rcbuff=HAL_CAN_Receive_IT(&hcan1,CAN_FIFO0);
 
HAL_UART_Transmit(&huart1,Rcbuff,15,10);
 
      HAL_Delay(100);
 
 
 
 }
 
}
 
 
 
 
static void MX_USART1_UART_Init(void)
 
{
 
 
 huart1.Instance = USART1;
 
 huart1.Init.BaudRate = 9600;
 
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 
 huart1.Init.StopBits = UART_STOPBITS_1;
 
 huart1.Init.Parity = UART_PARITY_NONE;
 
 huart1.Init.Mode = UART_MODE_TX_RX;
 
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 
   __HAL_UART_ENABLE_IT( &huart1,UART_IT_TXE) ;
 
 if (HAL_UART_Init(&huart1) != HAL_OK)
 
 {
 
   _Error_Handler(__FILE__, __LINE__);
 
 }
 
 
}
 
 
void SystemClock_Config(void)
 
{
 
 
 RCC_OscInitTypeDef RCC_OscInitStruct;
 
 RCC_ClkInitTypeDef RCC_ClkInitStruct;
 
 
 
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 
 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV5;
 
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 
 RCC_OscInitStruct.Prediv1Source = RCC_PREDIV1_SOURCE_PLL2;
 
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
 
 RCC_OscInitStruct.PLL2.PLL2State = RCC_PLL2_ON;
 
 RCC_OscInitStruct.PLL2.PLL2MUL = RCC_PLL2_MUL8;
 
 RCC_OscInitStruct.PLL2.HSEPrediv2Value = RCC_HSE_PREDIV2_DIV5;
 
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 
 {
 
   _Error_Handler(__FILE__, __LINE__);
 
 }
 
 
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 
                             |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 
 {
 
   _Error_Handler(__FILE__, __LINE__);
 
 }
 
 
 
 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
 
 
 
 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
 __HAL_RCC_PLLI2S_ENABLE();
 
 
 
 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
 
}
 
 
 
 
static void MX_CAN1_Init(void)
 
{
 
 
 hcan1.Instance = CAN1;
 
 hcan1.Init.Prescaler = 16;
 
 hcan1.Init.Mode = CAN_MODE_NORMAL;
 
 hcan1.Init.SJW = CAN_SJW_1TQ;
 
 hcan1.Init.BS1 = CAN_BS1_5TQ;
 
 hcan1.Init.BS2 = CAN_BS2_3TQ;
 
 hcan1.Init.TTCM = DISABLE;
 
 hcan1.Init.ABOM = DISABLE;
 
 hcan1.Init.AWUM = DISABLE;
 
 hcan1.Init.NART = DISABLE;
 
 hcan1.Init.RFLM = DISABLE;
 
 hcan1.Init.TXFP = DISABLE;
 
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 
 {
 
   _Error_Handler(__FILE__, __LINE__);
 
 }
 
 
}
 
 
 
 
static void MX_WWDG_Init(void)
 
{
 
 
 hwwdg.Instance = WWDG;
 
 hwwdg.Init.Prescaler = WWDG_PRESCALER_8;
 
 hwwdg.Init.Window = 0x40;
 
 hwwdg.Init.Counter = 0x40;
 
 hwwdg.Init.EWIMode = WWDG_EWI_DISABLE;
 
 if (HAL_WWDG_Init(&hwwdg) != HAL_OK)
 
 {
 
   _Error_Handler(__FILE__, __LINE__);
 
 }
 
 
}
 
 
 
 
static void MX_GPIO_Init(void)
 
{
 
 
 GPIO_InitTypeDef GPIO_InitStruct;
 
 
 /* GPIO Ports Clock Enable */
 
 __HAL_RCC_GPIOD_CLK_ENABLE();
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 
 HAL_GPIO_WritePin(nCAN2_STB_GPIO_Port, nCAN2_STB_Pin, GPIO_PIN_RESET);
 
 
 
 
 
 GPIO_InitStruct.Pin = HS_LS_IN_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 
 HAL_GPIO_Init(HS_LS_IN_GPIO_Port, &GPIO_InitStruct);
 
 
 GPIO_InitStruct.Pin = S2_IN_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 
 HAL_GPIO_Init(S2_IN_GPIO_Port, &GPIO_InitStruct);
 
 
 
 
 GPIO_InitStruct.Pin = nCAN2_STB_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 
 HAL_GPIO_Init(nCAN2_STB_GPIO_Port, &GPIO_InitStruct);
 
 
 
 GPIO_InitStruct.Pin = CAN2_ERR_IN_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 HAL_GPIO_Init(CAN2_ERR_IN_GPIO_Port, &GPIO_InitStruct);
 
 
 
 
}
 
 
 
 
 
 
void _Error_Handler(char *file, int line)
 
{
 
 
 while(1)
 
 {
 
 }
 
 
 
}
 
 
#ifdef USE_FULL_ASSERT
 
void assert_failed(uint8_t* file, uint32_t line)
 
{ 
 
 
}
 
#endif 
 
 
 
 

This is our code.

So some arbitrary delays, no interrupt or callback code, doesn't wait/check status and doesn't kick the watchdog.

Turns status to a pointer, outputs data from random pointer.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

ok.. we will check.. Thank you so much..