cancel
Showing results for 
Search instead for 
Did you mean: 

uprogrammed STM32F4

dominik
Senior
Posted on November 22, 2014 at 18:35

Hi

Are some PINs on an unprogrammed device high or low? I have an unprogrammed STM32F4 and a short circuit on the power supply 3.3V, therfore I can't program the chip...

Regards
2 REPLIES 2
Posted on November 22, 2014 at 18:50

Short-circuits would tend to be caused by solder, incorrect orientation of the part, and circuit design/fabrication failures.

More than one board?

An unprogrammed part is going to have the majority of it's signal lines in input mode, it will crash almost immediately as there is no valid code to execute. The run something you'd need to strap BOOT0 so it enters the System Loader.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dominik
Senior
Posted on December 21, 2014 at 20:59

Its ok, a component was soldered wrong. Thanks