2023-06-10 4:55 AM
I created many projects using CubeIDE1.9. I now installed CubeIDE1.12 and need to open my projects in the new version. I copied my old projects to a new workspace I created and then tried to import/open projects using CubeIDE1.12 but got a generic 'error' with no details when I try to open some of them.
How do I upgrade my projects from CubeIDE1.9 to CubeIDE1.12?
2023-06-11 1:25 AM
More details please? Windows or Linux? Which STM32?
Can you share an example project from CubeIDE 1.9?
2023-06-12 7:04 AM
The issue was resolved. It was related to the .cproject file having been duplicated from another project without renaming the contents. CubeIDE1.12 would quit with an unknown error.
I also had to use import 'Existing Projects into Workspace' instead of 'Projects from Folder or Archive'
2023-06-12 7:35 AM
Yes, this is not quite intuitive. When you want to import projects as is, without any conversion - use "Existing Projects into Workspace".
But I rarely, if ever, had to edit .cproject files for renaming a project.
Usually change of the name in .project file is enough.