2025-10-29 5:30 PM
Hi,
I'm using an STM32H750XBH6 with an ISSI IS42S32400J-6BL, but the read/write operations keep failing.
I’ve tried setting the CLK to 166 MHz / 120 MHz / 100 MHz / 50 MHz, but it still fails.
When measuring with an oscilloscope, I found that the FMC_Dx pins of the STM32H750XBH6 show an extra waveform in addition to the normal data waveform during output.
I disconnected the 22 Ω series resistors, but the same waveform can still be observed on the MCU’s FMC_Dx pins.
Does anyone know what might be causing this?
pic 1
2025-10-30 12:38 AM - edited 2025-10-30 12:48 AM
Hello @supen and welcome to the community;
Ensure that the hardware setup and clock frequency are correctly configured and verify signal integrity.
Could you please try to configure the IO speed very high.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.