cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750XBH6 Plan to use eMMC 8GB Kioxia THGBMJG6C1LBAU7 This eMMC is compliant with JEDEC/MMCA Version 5.1 interface with 1 I/O, 4 I/O and 8 I/O mode. Any potential problems? In manual for STM32H750XBH6 eMMC version is up to 4.x Thanks

BHell.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

It's not going to support the 5.x operational modes, you usually walk the parts into the mode both sides can support from the 1-bit 400 KHz starting point. You probe the CSD and EXTCSD to determine capacities, modes, etc. My expectation is that you'd run out of bandwidth on the STM32 long before you find the limit of the memory IC.

The eMMC BGA have a standard form factor, you should be able to find SD / MicroSD card adapters and clam-shell sockets to verify/validate use of specific parts.

Samsung, SanDisk, Toshiba, Kingston, and others work in fixturing I've done with other STM32, spanning into H7's

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..