cancel
Showing results for 
Search instead for 
Did you mean: 

Undefined reference in EEPROM emulation package

WSpar.1
Associate III

Hi all,

I'm trying to implement manually the ST EEPROM emulation package.

But I got stuck at a undefined reference:

0693W00000Dq7pRQAR.png 

I included in the right build paths and in the IDE I can perfectly jump to the EE_Init() function.

So the IDE does know where to look, but my compiler doesn't

What can be the problem here?

13 REPLIES 13
TDK
Guru

You need to add all directories with source files in them to the source folders.

Project properties -> C/C++ General -> Paths and Symbols -> Source Location

If you feel a post has answered your question, please click "Accept as Solution".

Go to the folder right above and right-click on that. By default the stuff shows in the tree but it not part of the build process.

Go to a folder above. Do it on Middlewares. Then you may have to refresh (F5) until you see the change. The Middlewares folder then gets the blue thing I think.

WSpar.1
Associate III

Thanks, that solved my problem.

Probably better to just select the project parent folder.