2018-11-29 8:42 PM
I want to power my B-L072Z (all in one LoRa module) with battery. i am able to power the board but not able to transmit/receive data. What should I do. Tell me any solution asap.
Thank you.
Regrd,
Sagar
2018-11-29 9:08 PM
>> What should I do.
Instrument the code, output diagnostic via a UART, and figure out what's happening.
The boards work with batteries, work out what you're doing wrong.
2018-11-29 9:36 PM
Thank you@Clive.
But I am not doing any extra thing. I just burned the Sample code (Given by semtech). Packets are transmitted successfully If I power the board with USB cable(Through PC).
But it doesn't work if I remove the USB power and insert the Batteries as a input power source.
Please help me out.
Regrd,
Sagar
2018-12-07 2:22 AM
Solution:
From UM2115 User manual "Discovery kit for LoRaWAN™ and LPWAN protocols with STM32L0":
"If the board is supplied by CN13, by battery or by CN11, SB37 must be removed to release the RESET pin managed by ST-LINK. In that case the ST-LINK is no more powered."
2021-12-22 2:24 PM
Hello.
I have the same problem but removed SB37 didn't solve it.
Is there something else to resolve it in order to use BL072z only with battery ?
Thanks a lot !