2025-03-16 11:28 PM
I am using an STM32G4 microcontroller with UCPD and the USBPD middleware. I was following this tutorial (same as AN5418 https://www.st.com/resource/en/application_note/dm00663511-how-to-build-a-simple-usbpd-sink-application-with-stm32cubemx-stmicroelectronics.pdf:(
https://youtu.be/-vsJhNIaHxE?si=3wosMAMXrO40mVZr
I, however, have a custom PCB without a TCPP chip, I'm not sure if this makes a difference. I set up everything according to the tutorial and I added the code it requires. Additionally, I added the following code to EvaluateSinkCapabilites:
void USBPD_DPM_SNK_EvaluateCapabilities(uint8_t PortNum, uint32_t *PtrRequestData, USBPD_CORE_PDO_Type_TypeDef *PtrPowerObjectType)
{
/* USER CODE BEGIN USBPD_DPM_SNK_EvaluateCapabilities */
USBPD_SNKRDO_TypeDef rdo;
rdo.d32 = 0;
/* Prepare the requested pdo */
rdo.FixedVariableRDO.ObjectPosition = 1;
rdo.FixedVariableRDO.OperatingCurrentIn10mAunits = 50;
rdo.FixedVariableRDO.MaxOperatingCurrent10mAunits = 50;
rdo.FixedVariableRDO.CapabilityMismatch = 0;
*PtrPowerObjectType = USBPD_CORE_PDO_TYPE_FIXED;
*PtrRequestData = rdo.d32;
//USBPD_HandleTypeDef *pdhandle = &DPM_Params[PortNum];
uint32_t size;
uint32_t snkpdolist[USBPD_MAX_NB_PDO]; // Array to store sink PDOs
USBPD_PDO_TypeDef pdo;
// Get the list of sink PDOs
USBPD_PWR_IF_GetPortPDOs(PortNum, USBPD_CORE_DATATYPE_SNK_PDO, (uint8_t *)snkpdolist, &size);
HAL_Delay(100);
ssd1306_Display(1);
ssd1306_Fill(Black);
ssd1306_SetCursor(0, 0);
ssd1306_WriteString("Available PDOs:", Font_11x18, White);
// Iterate through each sink PDO and print its details
for (uint32_t i = 0; i < size; i++)
{
pdo.d32 = snkpdolist[i]; // Get each PDO
char pdo_info[256]; // Adjust the size if needed
snprintf(pdo_info, sizeof(pdo_info), "%u mV, %u mA", pdo.SNKFixedPDO.VoltageIn50mVunits*50, pdo.SNKFixedPDO.OperationalCurrentIn10mAunits * 10);
ssd1306_SetCursor(0, 7 + i*7);
ssd1306_WriteString(pdo_info, Font_11x18, White);
}
ssd1306_UpdateScreen();
/* USER CODE END USBPD_DPM_SNK_EvaluateCapabilities */
}
I also have some code to manipulate the display in main() which is why I know the microcontroller is working. On a USB-A to USB-C cable nothing is changed on the screen, which means this function isn't getting called and its just getting 5V because its USB-A. On a USB C power supply it doesn't even turn on (no voltage is given), so I don't think this function is getting called or the negotiation is working at all, even though I've connected the UCPD CC lines to the port.
STM32CubeMx:
I would greatly appreciate if someone helped me debug this!
2025-03-17 2:03 AM - edited 2025-03-17 2:43 AM
Hi @Nv7
I, however, have a custom PCB without a TCPP chip, I'm not sure if this makes a difference.
> Sure, it makes big difference. The issue could be linked to your hardware implementation. Double-check the schematic and PCB layout to confirm that UCPD CC lines are correctly connected to the USB-C connector on your custom PCB. Would you attach a trace .cpd ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-17 7:37 AM
Yes, the CC lines on the USB port are connected to the chip's UCPD CC lines, although I don't have any resistors on those lines just a direct connection - is that how it's supposed to work? I'm, not sure how to make a trace.cpd file.
2025-03-26 5:07 AM
Hi @Nv7
I guess it's quite complex to follow your custom setup without testing it. I recommend using TCPP ports instead and x nucleo expansion board so that we can help you.
In general, the USB PD specification allows CC receiver (cReceiver) capacitance in the range of 200 pF to 600 pF.
For noise filtering purposes, an extra 390 pF +/- 10% capacitance must be added on each CC line close to the
TypeC connector.
When a TCPP0x is used, these capacitors must be added between the TCPP0x and the TypeC connector, as close to the Type-C connector as possible.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.