cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to program my GPIO image on STM32H750B-DK

nsingh
Associate II

Hi ,

I am not sure but my development board STM32H750B-DK may have some issues and I need some help to find what it may be . 

 

As per the readme.txt (there is very less literature that I could find on this board) , I could dump the ext_mem boot bin into the Internal flash and I did not face any issue there. I am now trying to flash the IO toggle image onto the QSPI flash present on the development board and I always face the same error. I feel that there maybe a hardware issue on the board but I could be wrong. Your help is highly appreciated. 

I have attached the error image. 

nsingh_0-1731845025347.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

@nsingh wrote:

I am not sure what is my external loader supposed to be . 


The NOR Flash (the first one).


@nsingh wrote:

Also, is it possible to get schematics of this board ?


The schematics: 

B04 version: https://www.st.com/resource/en/schematic_pack/mb1381-h750xb-b04.pdf

B01 version: https://www.st.com/resource/en/schematic_pack/mb1381-h750xb-b01-schematic.pdf

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Pavel A.
Super User

Can you connect to the board with CubeProgrammer and read from the internal flash?

Shirley.Ye
ST Employee

if you want to download the image into the QSPI, please make sure you have selected the external flash loader. Are you successfully download the image into the external flash before?

mÆŽALLEm
ST Employee

Hello @nsingh and welcome to the community,

Make sure you uploaded first the external boot firmware from Projects\STM32H750B-DK\Templates\ExtMem_Boot

Then upload the GPIO toggle example from: Projects\STM32H750B-DK\Examples\GPIO\GPIO_IOToggle

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
nsingh
Associate II

Thanks for your responses. 

I am not sure what is my external loader supposed to be . With the version 2.17 of the programmer , I could not find the external loader for STM32H750B-DK . Which one should I choose. I tried the second one but I still could not flash the image although I could fully erase the external flash.  Also, is it possible to get schematics of this board ?

nsingh_0-1731960431025.png

 

 


@nsingh wrote:

I am not sure what is my external loader supposed to be . 


The NOR Flash (the first one).


@nsingh wrote:

Also, is it possible to get schematics of this board ?


The schematics: 

B04 version: https://www.st.com/resource/en/schematic_pack/mb1381-h750xb-b04.pdf

B01 version: https://www.st.com/resource/en/schematic_pack/mb1381-h750xb-b01-schematic.pdf

Hope it helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Can you tell me which schematic version applies to the STM32H750B-DK ? The silkscreen says MB1381B 

You need to check that in your board :

SofLit_0-1732364621319.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.