cancel
Showing results for 
Search instead for 
Did you mean: 

unable to interface VL53L4CX with STM32F030

Anirudh_balaji
Associate II

Hi team,

 

I am new to the STM32 Cube IDE environment and would like to interface and control the VL53L4CX Time-of-Flight sensor using an STM32F030 DEMO Board. I kindly seek your guidance and support in achieving this.

 

Here are the details of the hardware I am working with:

 

I only have an STM32F030 DEMO Board to work with, When I try to do the Pin assignments for the MCU (STM32F030F4P6), by including the software pack X-CUBE-TOF1 in simple ranging mode; the BSP APIs for the pins TOF_INT_PIN and VL53L4CX_XSHUT are unknown, Please find the attached image for your kind reference,

 

 

Anirudh_balaji_4-1736401237886.png

 

Additionally, is vl53l4 only compatible with Nucleo boards? Correct me if I am wrong, but if that is not the case, can you please guide me in establishing communication between STM32F030 and VL53L4CX?

 

I am also available to schedule a call with the ST team to discuss and resolve this. I look forward to your support.

Thanks and Regards,

Anirudh

0 REPLIES 0