cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to install driver for STM32 nucleo board in windows 10

KA
Associate II

The driver is not getting installed in windows 10. The device driver installation wizard says it was unable to find any drivers designed for my machine. I am using Windows 10 version 1903.

2 REPLIES 2
TFlac
Associate III

Well, can't be 10% sure what is wrong, I will say that Windows 7 functions fine. One thing to note, your system has to be 64bit machine - I'm sure it is to run Windows 10. I loaded the Nucleo drivers on my computer with no problem. The next question is, what brand computer do you have. I only use IBM / Lenovo ThinkPad or ASUS.

I have a Windows 10 HP but never ran ST software. That machine only has 4GB of DRAM, I prefer 8GB. Take a look at your system. When I sit in the Hands-On-Labs there is always about thirty students and I don't see anyone having this problem.

TDK
Guru

Works fine for me. What driver are you installing? ST-Link? Go to the website and download it manually.

If you feel a post has answered your question, please click "Accept as Solution".