2023-03-26 11:34 PM
After powering STM32L151V8T6A device, I can't connect to the device. I try to connect by SWD or JTAG without success. Connect under reset doesn’t help. How can I connect the device?
2023-03-26 11:42 PM
Welcome, @OVill.1, to the community!
What tools are you trying to connect with, i.e. what hardware debugger and software are you using?
Regards
/Peter
2023-03-26 11:49 PM
Hello,
I am using the STLINK-V3 and the STM32CubeIDE Version: 1.11.2. For the debug proge, I use the ST-LINK GDB server.
Thanks and regards,
Olivier
2023-03-26 11:52 PM
...running on what OS?
2023-03-27 12:05 AM
In windows 10 Entreprise LTSC