cancel
Showing results for 
Search instead for 
Did you mean: 

UCPD Source(X_NUCLEO_SRC1M1) and Sink (X_NUCLEO_SNK)

Sudarshan
Associate

Hello,

We have purchased the following boards recommended by STM in order to work on UCPD Source and Sink applications:

1. Two NUCLEO-G071RB boards

2. One X-NUCLEO-SRC1M1

3. One X-NUCLEO-SNK1M1

We downloaded the repository of board and imported the following default examples from its pack: X-CUBE-TCPP (4.1.0) :

1. SRC1M1_Source

2. SNK1M1_Sink

But while logging the traces, we observe that Explicit Contract is not negotiated. I am sharing the traces from STM UCPD Monitor tool Ver 1.3.0 and also the test set-up.

Please suggest what else needs to be done in order to get the set-up working as desired.

With regard,

Sudarshan Chaudhary

3 REPLIES 3
FBL
ST Employee

Hi @Sudarshan 

It is recommended to never delete any content after addressing an issue or for any other reason. This can result in a loss of valuable information and effort, especially when investigating a problem.

Do you still have the same issue?  If it has been resolved, feel free to share the solution.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Since the set-up started working with few more tries in the same way as per the Default examples, I thought of removing my query from the STM forum. This was done considering that someone's precious time and efforts should not be put unnecessarily.

Thank you

Hi @Sudarshan 

Thank you for your understanding. As moderators, we recommend the good practice of leaving queries and their solutions on forums, even if they have been resolved. This helps others and contributes to the community's collective knowledge.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.