cancel
Showing results for 
Search instead for 
Did you mean: 

UART2 RX TX initialization

pietruha8
Associate II
Posted on December 18, 2011 at 16:29

UART2 RX TX initialization-how to use?

Hello, I have problem with initialization UART2 in my project(STM8S105). Below you can see part of my code, what am i doing wrong?

I'm trying to send sign to LCD display.

[code]

void UART2_Cmd(FunctionalState ENABLE);

void UART2_InitGPS()

{

    UART2_DeInit();

    UART2_Init( (u32)9600, UART2_WORDLENGTH_8D, UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE);   

}

void UART2_SendData8(u8 Data);

u8 UART2_ReceiveData8(void);

void main(void)

{

    char tmp;

    LCD5110_init();

//function which initialize LCD

    LCD5110_set_XY(0,0);

//function which set rows and columns in LCD

    UART2_SendData8(36);

    UART2_ReceiveData8();

    tmp = UART2_ReceiveData8();

    LCD5110_write_char(tmp); //function which send characters to LCD

}

[/code]

I have to mention that i have no errors after compiling code and if I use function like this everything works fine(but I need UART to racive data from GPS and send it to LCD) :

[code]

void main(void)

{

    char tmp=33; //33 -> ''!'' sign in my matrix(table or haw to name it)

    LCD5110_init();

//function which initialize LCD

    LCD5110_set_XY(0,0);

//function which set rows and columns in LCD

  

    LCD5110_write_char(tmp); //function which send characters to LCD

}

[/code]

BR,

Konrad

P.S. If somebody wants to see whole code let me know :)

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on December 19, 2011 at 01:11

This isn't an STM8 forum.

Consider if the GPS is using 9600 8N1, a lot use 4800 8N1

Consider sending data in a loop, GPS sentences are often 80-100 characters in length, so you forward more than one character.

In embedded you typically don't want to exit the main() subroutine.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pietruha8
Associate II
Posted on December 19, 2011 at 23:46

Yes I know but I've had no answers on STM8 so I tried here. Thanks for answer, Stm8 are using 9600, I have it from examples. I'll try to send more data and let you know.

pietruha8
Associate II
Posted on December 21, 2011 at 20:04

GPS is not connected now, i'm trying to send data in loop -> from PD5(UART2 Tx pin) to PD6

(UART2 Rx pin), trap is set in ''

LCD5110_write_char(gp);

'' line and i see that 'gp' variable is empty...

void UART2_Init();

void UART2_Cmd();

void GPIO_Init();

void UART2_SendData8(u8 Data);

u8 UART2_ReceiveData8(void);

void main(void)

{

    char gp;

    char i;

    u8 Data='k';

    LCD5110_init();

    LCD5110_set_XY(1,1);

    UART2_Init( (u32)9600, UART2_WORDLENGTH_8D, UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE);

    UART2_Cmd(ENABLE);

    GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST );

    GPIO_Init(GPIOD, GPIO_PIN_6, GPIO_MODE_IN_FL_NO_IT );

    UART2_SendData8(Data);

    UART2_ReceiveData8();

    gp = UART2_ReceiveData8();

    LCD5110_write_char(gp);

}

Posted on December 21, 2011 at 20:38

Aren't you supposed to wait for the status to indicate a character is ready before reading it from the data register.

Receive:

while(UART2_GetFlagStatus(UART2_FLAG_RXNE) == RESET);

data = UART2_ReceiveData8();

Transmit:

UART2_SendData8(byte);

while(UART2_GetFlagStatus(UART2_FLAG_TXE) == RESET);

BTW ST I really hate this stupid Word(tm) editor

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pietruha8
Associate II
Posted on December 21, 2011 at 21:10

I don't get it, where should I put those functions in this code?

pietruha8
Associate II
Posted on December 21, 2011 at 21:15

AAAAA! I love you man! :) thanks :) It seems to be working now. Ok i will try to do some more things ... just to be sure

void UART2_Init();

void UART2_Cmd();

void GPIO_Init();

void UART2_SendData8(u8 Data);

u8 UART2_ReceiveData8(void);

void main(void)

{

    int gp;

    u8 data;

    u8 byte=66;

    LCD5110_init(); //inicjalizacja LCD

    LCD5110_set_XY(1,1); //ustawienie R i C

    UART2_Init( (u32)9600, UART2_WORDLENGTH_8D, UART2_STOPBITS_1, UART2_PARITY_NO, UART2_SYNCMODE_CLOCK_DISABLE, UART2_MODE_TXRX_ENABLE); //Inicjalizacja UART2

    UART2_Cmd(ENABLE); // Warunek konieczny do send i recieve

    GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST );// przypisanie pinow

    GPIO_Init(GPIOD, GPIO_PIN_6, GPIO_MODE_IN_FL_NO_IT );

    //UART2_SendData8(data);

    UART2_SendData8(byte);

  while(UART2_GetFlagStatus(UART2_FLAG_TXE) == RESET);

    //UART2_ReceiveData8();

    while(UART2_GetFlagStatus(UART2_FLAG_RXNE) == RESET);

  data = UART2_ReceiveData8();

    gp = UART2_ReceiveData8();

    LCD5110_LCD_write_byte(gp, 1);

}