2025-08-01 1:20 AM - edited 2025-08-01 1:22 AM
Hi,
I am using STM32Cube_FW_H5_V1.5.0.
I initialize a MPU region with the following code, using only LL-calls:
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER6, LL_MPU_REGION_PRIV_RW|LL_MPU_INSTRUCTION_ACCESS_DISABLE|LL_MPU_ACCESS_NOT_SHAREABLE, LL_MPU_ATTRIBUTES_NUMBER2, 0x90000000U, 0x9FFFFFFFU);The corresponding MPU register MPU_RLAR_Ax gets set to 0x9FFFFFE3, wich is obviously wrong because I wanted to select attribute#2 and instead the attribute field gets set to 0x1.
For verification I did the same initialization using HAL-calls:
MPU_Region_InitTypeDef region;
region.Enable = MPU_REGION_ENABLE;
region.Number = MPU_REGION_NUMBER6;
region.AttributesIndex = MPU_ATTRIBUTES_NUMBER2;
region.BaseAddress = 0x90000000U;
region.LimitAddress = 0x9FFFFFFFU;
region.AccessPermission = MPU_REGION_PRIV_RW;
region.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
region.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
HAL_MPU_ConfigRegion(®ion);Now the MPU register MPU_RLAR_Ax gets set to the correct value of 0x9FFFFFE5.
I think the bug is within the LL_MPU_ConfigRegion() code. The current implementation of this function in fw1.5.0 is:
__STATIC_INLINE void LL_MPU_ConfigRegion(uint32_t Region, uint32_t Attributes, uint32_t AttrIndx, uint32_t BaseAddress,
uint32_t LimitAddress)
{
/* Set region index */
WRITE_REG(MPU->RNR, Region);
/* Set region base address and region access attributes */
WRITE_REG(MPU->RBAR, ((BaseAddress & MPU_RBAR_BASE_Msk) | Attributes));
/* Set region limit address, memory attributes index and enable region */
WRITE_REG(MPU->RLAR, ((LimitAddress & MPU_RLAR_LIMIT_Msk) | AttrIndx | MPU_RLAR_EN_Msk));
}where line 11 should be changed to:
WRITE_REG(MPU->RLAR, ((LimitAddress & MPU_RLAR_LIMIT_Msk) | (AttrIndx << 1) | MPU_RLAR_EN_Msk));
}A change of the LL_MPU_ATTRIBUTES_NUMBERx definitions might be another option to solve this, but might have a major impact on the rest of the firmware pack since these definitions are used in a lot of places.
Thank you very much for confirming this bug. If it is a real bug and not a miss-interpretation on my side I would be very happy to see it fixed eventually.
Best Regards
Thomas
Solved! Go to Solution.
2025-08-01 2:44 AM
Hello @TThan
Thank you for reporting this point. An internal ticket is created in order to investigate and fix this potential defect (ticket number 215184)
With regards
2025-08-01 2:44 AM
Hello @TThan
Thank you for reporting this point. An internal ticket is created in order to investigate and fix this potential defect (ticket number 215184)
With regards