2011-12-21 3:45 AM
How can I synchronize the timer output with a maximum frequency PLL,
ie 168 MHz. In my example I set the timer to slow generate an interrupt, which run fast timer for generating a single pulse duration of 6 ns, but I have a jitter of 10 ns. Example my codes: 1) /* Time base configuration TIM9 (fast)*/ TIM_TimeBaseStructure.TIM_Period = 100; TIM_TimeBaseStructure.TIM_Prescaler = 0; // max freq. (168 MHz) TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM9, &TIM_TimeBaseStructure); /* TIM9 PWM2 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 100;//get pulse ~6ns TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM9, &TIM_OCInitStructure); /* One Pulse Mode selection */ TIM_SelectOnePulseMode(TIM9, TIM_OPMode_Single); /* Time base configuration TIM3 (slow) */ TIM_TimeBaseStructure.TIM_Period = 1000; TIM_TimeBaseStructure.TIM_Prescaler = 8; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel4 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; // pulse for control TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC4Init(TIM3, &TIM_OCInitStructure); //TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM3, ENABLE); /* TIM Interrupts enable */ TIM_ITConfig(TIM3, TIM_IT_CC4 , ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); 2) config output pins /* TIM3 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* Enable peripheral clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOE, ENABLE); /* TIM9 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM9, ENABLE); /* TIM3_CH4 pin (PC.09) configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); /* TIM9_CH1 pin (PE.05) configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOE, &GPIO_InitStructure); 3) interrupt config /* Enable the TIM3 gloabal Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); 4) interrupt routine void TIM3_IRQHandler(void) { if (TIM3->SR & TIM_IT_CC4) // { /* Clear the IT pending Bit */ TIM3->SR &= ~TIM_IT_CC4; TIM9->CR1 |= TIM_CR1_CEN; // start new pulse } } TIM9_CH1 (PE.05) output should be synchronized with TIM3_CH4 (PC.09) oputput, but it don't. How to fix this trouble? #stm32f4-discovery2011-12-21 8:39 AM
The values for Prescale and Period take the form (N - 1)
For 1000 cycles, use 999 Pulse of 0 is always OFF, 1000 is always ON Period = 100 - 1; // 100 cycles Pulse = 99; // Low for a single tick, High for 99 (out of 100)2011-12-21 9:09 AM
Thanks! B
ut
I installed the
other
pulse durations
, the jitter
is still
present.
2011-12-21 11:10 AM
If it is jitter, then I'd start by using clock sharing a common divider source (ie APB2) and the same prescaler.
A jitter of ~6ns suggests its falling on either side of an odd divider (asymmetrical duty cycle)