2024-10-15 11:16 AM - edited 2024-10-15 11:18 AM
Hi,
i wrote code that wait for a ping from esp32 and when he got it, it sent back pong to esp32
In the uart1 everthing works fine, but i do not understand why, in uart2 it is not working
I doubled checked the code and everthing looks ok for me,
The code is the same like uart1, i just changed everything from uart1 to uart2
Code in uart2 - Not Working:
#include "stm32f4xx.h"
#include <string.h>
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;
uint8_t rxBuffer[5] = {0}; // Buffer for receiving data
const char *ping = "PING";
const char *pong = "PONG";
/* Function Prototypes */
void SystemClock_Config(void);
void Error_Handler(void);
void GPIO_Init(void);
void USART2_UART_Init(void);
/**
* @brief The application entry point.
* @retval int
*/
int main(void) {
/* Initialize the HAL Library */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize GPIO pins and USART2 */
GPIO_Init();
USART2_UART_Init();
while (1) {
// Receive 4 bytes (expecting "PING")
HAL_UART_Receive(&huart2, rxBuffer, 4, HAL_MAX_DELAY);
// Compare received data to "PING"
if (strncmp((char *)rxBuffer, ping, 4) == 0) {
// If "PING" received, send "PONG" back
HAL_UART_Transmit(&huart2, (uint8_t *)pong, strlen(pong), HAL_MAX_DELAY);
}
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
void GPIO_Init(void) {
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Enable GPIO clock for PA2 and PA3 (USART2 TX/RX pins) */
__HAL_RCC_GPIOA_CLK_ENABLE();
/* Configure PA2 (USART2 TX) */
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; // Alternate function push-pull
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2; // AF7 for USART2
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Configure PA3 (USART2 RX) */
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; // Alternate function push-pull
GPIO_InitStruct.Pull = GPIO_PULLUP; // Enable pull-up for RX
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2; // AF7 for USART2
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
void USART2_UART_Init(void) {
/* Enable USART2 clock */
__HAL_RCC_USART2_CLK_ENABLE();
/* Initialize USART2 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK) {
Error_Handler(); // Handle initialization error
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void) {
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/* Configure the main internal regulator output voltage */
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/* Initializes the RCC Oscillators according to the specified parameters */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 100;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
/* Initializes the CPU, AHB and APB buses clocks */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK |
RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) {
Error_Handler();
}
}
/**
* @brief This function is executed in case of error occurrence.
*/
void Error_Handler(void) {
while (1) {
// Stay in a loop if there is an error
}
}
Thanks for your help
2024-10-15 4:05 PM
Hi,
Is 9600 baud the correct speed for ESP32?
Kind regards
Pedro
2024-10-15 10:51 PM - edited 2024-10-15 10:52 PM
Hi,
Of course, if i was not define 9600 also in esp32 then the uart1 also was not worked.
This is the code i wrote in the esp32:
2024-10-15 10:58 PM
Hi, maybe the cause is because your clock for USART1 and USART2 is different, for USART1 the clock is form APB1 but for USART2 the clock is from APB2, so the BaudRate is different, you can check it.
2024-10-15 11:01 PM - edited 2024-10-15 11:01 PM
You can see in the full code i sent of the stm32: (I paste here just the part of the clocks)
void SystemClock_Config(void) {
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/* Configure the main internal regulator output voltage */
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/* Initializes the RCC Oscillators according to the specified parameters */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 100;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
/* Initializes the CPU, AHB and APB buses clocks */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK |
RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) {
Error_Handler();
}
}
I see now that there is also RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2
Do i need to remove it or modifiy it?
2024-10-15 11:10 PM
Hi, I mean you can modify 'RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2' too (same as APB1), then to try again.
2024-10-15 11:25 PM
Hi,
The code is the same like uart1, i just changed everything from uart1 to uart2
Did you just use find-n-replace "uart1" with "uart2" in main.c ?
Kind regards
Pedro
2024-10-15 11:38 PM - edited 2024-10-15 11:57 PM
actually i asked from chat gpt to change from uart1 to uart2, and then it regenerate the code for uart2
2024-10-15 11:56 PM
Still no working
2024-10-16 12:04 AM
hahahaha, that's funny... Good luck!