UART stm32F767ZI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-19 11:25 AM
Hello everybody,
i wanted to send data from realterm serial to the stm32F767ZI but it dose not work. i cant see any message on my terminal. The same code is working good with STMF446re. The UART2 with STM32F4446re is connected to the USB Port. but with stm32F767ZI i am not sure and i searched in datasheet to find any info but i did not find. please i need your help.
#[UART/USART]​ #I2C​
- Labels:
-
I2C
-
STM32F7 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-19 11:43 AM
Perhaps try looking at the F7 HAL code examples?
The NUCLEO-F767ZI likely uses a different USART and pins.
//****************************************************************************
void OutChar(char c)
{
while((USART3->ISR & USART_ISR_TXE) == 0); // Wait for Empty
USART_RS232->TDR = c; // Send Char
}
//****************************************************************************
void USART3_Init(void) // USART3 PD8/PD9 NUCLEO VCP
{
GPIO_InitTypeDef GPIO_InitStruct = { 0 };
UART_HandleTypeDef UartHandle = { 0 };
__USART3_CLK_ENABLE();
__GPIOD_CLK_ENABLE();
/* UART RX/TX GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_8 | GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*## Configure the UART peripheral ######################################*/
/* Put the USART peripheral in the Asynchronous mode (UART Mode) */
/* UART1 configured as follow:
- Word Length = 8 Bits
- Stop Bit = One Stop bit
- Parity = NO parity
- BaudRate = 115200 baud
- Hardware flow control disabled (RTS and CTS signals) */
UartHandle.Instance = USART3;
UartHandle.Init.BaudRate = 115200;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
#ifdef UART_ONE_BIT_SAMPLE_DISABLE
UartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
#endif
if (HAL_UART_Init(&UartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
//****************************************************************************
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
‎2019-05-19 12:24 PM
Assuming you are using the same UART and that is valid on the same port/pinno combinations then it is almost certainly the alternate function setting.
For example UART 5 on the H743 and F767 can both be PB12/PB13 but one is GPIO_AF14_UART5 and the other GPIO_AF8_UART5
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-19 1:16 PM
Compare the UART register description in the reference manuals to see if both come from the same design IP version.
SPI has 3 versions, UART probably 2+ (one on the H7 has FIFOs)