UART Receive issue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-30 3:37 AM
Hello,
I'm struggling with a really strange issue. I'm trying to make UART RX working on a STM32G4 custom board.
I've followed the UART Interrupt tutorial. (https://wiki.st.com/stm32mcu/wiki/Getting_started_with_UART)
I've tested it with Nucleo-G431RB and it works fine.
Now I'm running the exact same code on my custom board and I have nothing, when using the debugger I can see that the interrupt is never fired. I've check hardware connections and everything seems OK.
I've also tried to implement UART_Receive by polling mode => I can see in the debugger that characters are received, so Hardware is OK.
Can someone help me with this issue ?
Thanks
Solved! Go to Solution.
- Labels:
-
STM32G4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-10-31 10:17 AM
Why ST couldn't have used a symbol for the vector table basis into SCB->VTOR is honestly beyond me...
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
‎2023-10-31 1:14 PM
Your code you've posted is working on my Nucleo-G431B just fine.
With the exception is that you should use strlen instead of guessing the length of the string. I was getting some null characters when i sent SONAR.
Also remove the flag as i was getting double "msg_available"
Now you're probably wondering why I was able to get your code to work? I saw the link to the tutorial and nowhere did it mention to enable the NVIC interrupt. How ST left that vital information out is beyond me?
TimerCallback tutorial! | UART and DMA Idle tutorial!
If you find my solution useful, please click the Accept as Solution so others see the solution.

- « Previous
- Next »