cancel
Showing results for 
Search instead for 
Did you mean: 

UART interrupt not received after some time and ORE bit is high

vchau.2
Associate III

Hi All,

My application sends and receive data very frequently, Some times Tx and Rx may be occur same time, Application run for some time (10 sec or 20 sec) but after some time Rx interrupts stop working and i found ORE bit high.

So My question is

  1. What happen when Tx and Rx occur at same time (Tx blocking mode and Rx in interrupt mode)
  2. How to clear ORE bit it goes high
5 REPLIES 5

There's no reason RX and TX can't occur concurrently.

If your IRQ Handlers block for more than a byte time, you'll likely run into issues. Have them buffer data, and have whatever parsing/processing done somewhere else, that doesn't have tight time constraints.

Overruns occur if you are not attentive to hard deadlines.

Depends on the model of STM32, the Reference Manual should describe how to clear, and which register to use.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Which STM32?

> How to clear ORE bit it goes high

This is why it's important to tell, which STM32. There are 2 different UART modules in the various STM32 and the procedure is different too - but in any case, it's in the RM, so it's enough to read it and follow it.

0693W00000aHX2hQAG.png0693W00000aHX3QQAW.png 

So, check in the RM for *your* STM32.

JW

Karl Yamashita
Lead III

More than likely you don't check for HAL status when you call HAL_UART_Receive_IT. If it returns HAL_BUSY then the interrupt isn't enabled.

If that is the case, then check this post that i replied to https://community.st.com/s/question/0D53W000022Hi9ySAC/stm32-hal-uart-receive-interrupt-stops-receiving-at-random-times

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.
vchau.2
Associate III

Thanks for your answers,

As per data sheet USART is full duplex, I want to know if There is single register for Tx and Rx that is DR register, how can be full duplex, What else if Tx and Rx occur at a same time?

Its not a memory, the receive and transmit registers can exist at the same address, but there are two independent data paths and registers. The operate independently and concurrently.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..