cancel
Showing results for 
Search instead for 
Did you mean: 

Typos in the STM32L073x8 STM32L073xB STM32L073xZ datasheet DS10685 Rev 7

Todd1
Associate

p.14: Figure 1. The "DAC2-->OUT1" connection should rather be "DAC2 --> OUT2", or better still "DAC1 --> DAC_OUT1" and "DAC2 --> DAC2_OUT".

p.24: Section 3.5 Clock management, the System clock source bullet mentions "Three different clock sources..." but the third indent bullet for "- Multispeed internal RC oscillator (MSI),..." seems to be omitted.

p.26: Figure 2. Clock tree includes "LSU", "LSD", "LSD", and "LSD" signals between the @V33 block and @V18 block. "LSU" is not included in the figure's abbreviations Legend. It also looks like the first "LSD" should rather be "LSE", the second "LSD" should be "LSI", and the third "LSD" should be "LCDCLK".

p.50: Table 16. 48-Pin, pin #25 lists an alternate function "I2C2_SMBA" but SMBus is not supported on I2C2 per Table 12 on p.35 and a notation just above the table.

p.57: Table 18. Port B, PB12, also lists alternate function "I2C2_SMBA" but SMBus is not supported on I2C2 per Table 12 on p.35 and a notation just above the table.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KDJEM.1
ST Employee

Hi @Todd​,

Thank you for reporting these typos.

I confirm these confusions and I will check internally.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hello @Todd​ ,

Thanks for highlighted these typos.

I reported internally.

It will be fixed in the coming releases.

Internal ticket number: 145920 (This is an internal tracking number and is not accessible or usable by customers).

Thank you. 

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.