2021-03-28 8:20 PM
Hi,
I am using a text area to display a precision timer output (double) and need 8 decimal places of precision. Thye best I can get is six:
I have a wildcard buffer of twenty and the following code:
/* Backend code */
typedef struct
{
volatile uint32_t timerCountUpperWord;
volatile uint64_t clockTimerT1;
uint64_t clockBeatCount;
uint8_t clockTenBeatCounter;
uint16_t clockTenMinuteCounter;
uint32_t clockFourHourCounter;
uint64_t tenTickStartTime;
uint16_t tenMinuteBeatCount;
uint32_t fourHourBeatCount;
double tenTickBPM;
uint64_t tenMinuteStartTime;
double tenMinuteBPM;
uint64_t fourHourStartTime;
double fourHourBPM;
uint8_t tenTicksComplete;
uint8_t tenMinutesComplete;
uint8_t fourHoursComplete;
uint8_t resetBPMFlag;
uint8_t runFlag;
uint8_t runInitFlag;
uint8_t progInd10Ticks;
uint8_t progInd10Minutes;
uint8_t progInd4Hours;
}timerData_t;
timerData_t tData;
/*Touchgfx Code */
Unicode::snprintfFloat(textBPM_10TicksBuffer, TEXTBPM_10TICKS_SIZE, "%03.8f", tData.tenTickBPM);
The best I get is 90.056274 which is six decimal places.
If I change the code to:
Unicode::snprintfFloat(textBPM_10TicksBuffer, TEXTBPM_10TICKS_SIZE, "%03.12f", tData.tenTickBPM);
I get the same precision:
89.988746.
Which is 6 decimal places.
What am I doing wrong?
2021-03-29 4:32 AM
What is the value of TEXTBPM_10TICKS_SIZE?
Sorry, missed you mentioned the 20 characters above.
2021-03-29 4:32 PM
Hi Peter,
The size of the buffer was the first thing I thought of that's why I made it larger than I needed at 20.
Love the Touchgfx package. It took me about two days to get to grips with the basics. Once you get the hang of it Touchgfx is great easy to use, powerful and it produces great looking interfaces.
Before TGFX i used mobile phones with Blutooth or WiFi and custom apps for a decent interface, with Touchgfx that's no longer necessary. Using custom phone apps is a pain as you have to do Android and Apple. I used B4x for this as it is excellent for people who don't want to program in Java. Where I still need a phone app I will continue to use B4x.
Congratulations go to ST and Draupner Graphics for making such an excellent package available to everyone.
I will publish the project I'm working on at the moment at it may be useful to others starting up with Touchgfx.
Best regards
Rob
2021-03-30 10:48 AM
"%03.12f"
The number preceding the dot ("3" in this case) is not a number of digits before the decimal separator. It's a minimum number of total characters (not digits!) printed for the particular field.
2021-03-30 9:25 PM
Yes,
I know that is what it is supposed to be as per the documentation:
https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_unicode/#snprintffloat
Viz:
\%[flags][width][.precision]f
If I write
\%[flags][width][.precision]f
"%011.8f"
0089.988723
If I try:
"%013.8f"
I get:
000089.988723
The floating point number being displayed is: 89.98872391054008 using STM32CubeIDE Live Watch variable.
It simply does not work like the normal C /C++ printf or the Touchgfx snprintfloat documentation.
I have checked the layout an I am not truncating it in the display.
In this case the reading was 90.943244
The textArea extends out to the yellow border near the wren's tail so there is plenty of room for more another two digits.