2017-11-06 7:22 AM
Solved! Go to Solution.
2017-11-07 6:15 AM
Signal looks awful, try putting scope probe in 10x mode.
2017-11-07 6:17 AM
Check optimization level on compiler. Consider using pointer.
What toolchain?
2017-11-07 6:22 AM
Looks very much like you're hitting the limits of your measurement setup, i.e. scope bandwidth and (more probably) probe bandwidth - unless there's some limitation imposed by the PCB and/or connected circuitry, too.
Is it a 1:10 probe?
Also, from which memory are you running? Did you confirm your system clock runs at the frequency you assume it does?
JW
2017-11-07 6:23 AM
Clive One wrote:
Check optimization level on compiler. Consider using pointer.
What toolchain?
The best thing to find out whether this is the issue is to see the disasm.
JW
2017-11-07 6:37 AM
Completely agree, I'll see if I can find some that have higher limits, It's a 1:10 Probe (60 MHz) and a TDS3014C 100 MHz oscilloscope. Measuring directly onto the pins on the dev board at this point.
I checked the system clock, outputted a prescaler onto the RCC_MCO_2 and it was definitely at 216 MHz.
2017-11-07 6:40 AM
I'm running atollics truestudio with the following:
2017-11-07 6:40 AM
I implemented it with a 10x probe, didn't look any better, I might be hitting the probe limits, I'll try and get a higher bandwidth probe
2017-11-07 7:38 AM
This completely solves it, I thought the probe was 100 MHz as well until you pointed it out. Got a higher MHz probe and just measured a 109 MHz signal.
Thank you for all the help.
Sometimes its not the mcu but rather how we're trying to observe the mcu.
2017-11-07 8:27 AM
2017-11-07 8:46 AM
Something is still too slow. If you want to see 50MHz square wave correctly you need to have 3*50MHz and 5*50MHz or more harmonics too.