cancel
Showing results for 
Search instead for 
Did you mean: 

Timer STM32f4

fiulala
Associate II
Posted on February 23, 2015 at 23:20

Hello I want to generate pulses on a pin using a timer

. I would like to configure it so it could make, for example, 10 pulses and then stop. How do I have to configure the timer to do so?

 Using Counter Mode Down maybe? How should the ma�n look like?

Thank you very much

#stm32f4 #groundhog-day #timers #discovery
1 REPLY 1
Posted on February 24, 2015 at 00:34

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Stop%20PWM%20output%20after%20N%20steps&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=1746]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FStop%20PWM%20output%20after%20N%20steps&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1746

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..