Senior III
April 5, 2024
Question
Timer pwm complementary for BLDC
- April 5, 2024
- 1 reply
- 1018 views
I trying to figure out, how i should set up the complementary channels to achieve the signals, shown in the picture.
If i would activate them (tim_oc1n), they would have a pwm, like the normal channel (just inverted). So i think it is only possible to switch them between off state run mode ( OSSR - high or low) and normal pin configuration (high or low). But doing this, i can just use the normal pin function anyway.
Did i miss something?