2025-01-23 04:30 AM
Dear All,
I would like to interface an ADC (ADS131M08) with a STM32F407. The ADC datasheet mentions that for better performance, the ADC clock should be synchronized with the SPI clock. Is there any way to achieve such synchronization with the STM? I was thinking about a timer that can give the clock to the ADC and get this timer sync with the SPI, but I don't really see if it's possible and how to implement it.
Thanks for your help
Best regards
2025-01-23 08:39 AM
Hello @Yves_P,
You can use one of the timers to generate the ADC clock signal; configure the timer to generate a PWM signal at the desired ADC clock frequency. Then, set the SPI peripheral to operate at a frequency that is a multiple or sub-multiple of the ADC clock frequency
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.