2018-11-30 3:53 PM
I am using 32bit TIM5 in an STM32F469I. I enable the timer and divide the 8M clock by 1000000 to get microseconds. I then use microseconds to time pulses coming into the board from external device. All works well until the timer overloads. I can test this as I save the current and previous timer counts. When the current is less than the previous in count, I know it overloaded.
I thought that TIM5, a 32 bit timer, should reload on overflow. Once it overloads, it seems to go into a 16bit mode, I don't know, but the counts are lower than expected. They look like miliseconds at most instead of microseconds. Since all this is in an interrupt it is hard to tell.
Here's how I set the timer up. And by the way, all is well for about a minute, which would coincide roughly with the overflow as well. Ignore any subtle spelling errors as I had to type this in instead of copy/paste
__HAL_RCC_TIM5_CLK_DISABLE(); // tried with and without this statement
__HAL_RCC_TIM5_CLK_ENABLE();
TIM5->PSC=HAL_RCC_GetPCLK1Freq() / 1000000-1; // Clock should return 8,000,000
TIM5->CR1=TIM_CR1_CEN | TIM_CR1 | TIM_CR1_ARPE; // Tried with/without TIM_CR1_ARPE as it shouldn't be needed
I then read the timer with:
mctime = TIM5->CNT;
mctime counts up to a large 32bit number and then overflows and after that, slowly counts. At overflow I tried disabling the timer and re-enabling it. Maybe something else is using TIm5 on the board but I can't find it.
Pointers?
Thanks,
Jerry
2018-11-30 4:57 PM
TIM5->ARR is set to what?
This stuff is hard to remotely troubleshoot with incomplete code, no code showing diagnostic output, and no output to review.
2018-11-30 5:07 PM
ARR is set to 0xffffffff;
At initialization, the only difference I can see between then and at overflow is that init has SR=0x00 and at overflow SR = 0x1f;
CR1 is 0x81;
CNT is random depending on when it stops;
PSC = 0x29;
DMAR = 0x81;
Everything else is 0x00;
Do I need to clear the Status Register SR at overflow?
Thanks for trying.
Jerry
2018-11-30 6:49 PM
Is there something I should be doing in the interrupt at overflow? I've been debugging this all afternoon without luck.
thanks
2018-11-30 7:35 PM
>>Do I need to clear the Status Register SR at overflow?
Are you interrupting?
If you want to see each Update event flagged, you'd want to clear the first one, ie TIM5->SR = 0xFFFE;
Don't have an F469I that's not in use
Here TIM5 cycling on an F7, rolls every 43, doesn't filp into 16-bit mode
Hello World!
Prescaler 0
0 : 3
1 : 100090821
2 : 200190821
3 : 300290819
4 : 400390819
5 : 500490821
6 : 600590821
7 : 700690821
8 : 800790821
9 : 900890821
10 : 1000990821
11 : 1101090821
12 : 1201190821
13 : 1301290821
14 : 1401390819
15 : 1501490819
16 : 1601590821
17 : 1701690821
18 : 1801790821
19 : 1901890821
20 : 2001990821
21 : 2102090821
22 : 2202190819
23 : 2302290821
24 : 2402390821
25 : 2502490821
26 : 2602590821
27 : 2702690821
28 : 2802790821
29 : 2902890821
30 : 3002990821
31 : 3103090821
32 : 3203190821
33 : 3303290821
34 : 3403390819
35 : 3503490821
36 : 3603590819
37 : 3703690819
38 : 3803790819
39 : 3903890821
40 : 4003990821
41 : 4104090819
42 : 4204190821
43 : 9323525
44 : 109423525
45 : 209523525
46 : 309623523
47 : 409723525
48 : 509823525
49 : 609923525
50 : 710023523
51 : 810123525
52 : 910223525
53 : 1010323525
54 : 1110423525
55 : 1210523525
56 : 1310623523
57 : 1410723525
58 : 1510823525
59 : 1610923525
60 : 1711023523
61 : 1811123525
62 : 1911223525
63 : 2011323525
64 : 2111423523
65 : 2211523525
66 : 2311623525
67 : 2411723523
68 : 2511823525
69 : 2611923523
70 : 2712023525
71 : 2812123525
72 : 2912223525
73 : 3012323525
74 : 3112423525
75 : 3212523525
76 : 3312623525
77 : 3412723525
78 : 3512823525
79 : 3612923523
80 : 3713023525
81 : 3813123525
82 : 3913223525
83 : 4013323525
84 : 4113423525
85 : 4213523525
86 : 18656229
87 : 118756229
88 : 218856229
89 : 318956229
90 : 419056229
91 : 519156229
92 : 619256229
93 : 719356229
94 : 819456229
95 : 919556229
96 : 1019656229
97 : 1119756227
98 : 1219856227
99 : 1319956229
100 : 1420056229
101 : 1520156229
102 : 1620256227
103 : 1720356227
104 : 1820456229
105 : 1920556229
106 : 2020656227
107 : 2120756229
108 : 2220856229
109 : 2320956227
110 : 2421056227
111 : 2521156229
112 : 2621256229
113 : 2721356229
114 : 2821456229
115 : 2921556229
116 : 3021656229
117 : 3121756229
118 : 3221856227
119 : 3321956229
120 : 3422056229
121 : 3522156227
122 : 3622256229
123 : 3722356229
124 : 3822456229
125 : 3922556229
126 : 4022656229
127 : 4122756229
128 : 4222856227
129 : 27988933
130 : 128088933
131 : 228188931
132 : 328288933
133 : 428388933
134 : 528488933
135 : 628588933
136 : 728688933
137 : 828788933
138 : 928888933
139 : 1028988933
140 : 1129088933
141 : 1229188933
142 : 1329288933
143 : 1429388933
144 : 1529488931
145 : 1629588933
146 : 1729688933
147 : 1829788933
148 : 1929888933
149 : 2029988933
150 : 2130088933
2018-11-30 7:53 PM
all I need is the continuous count. I need a more granular time than what is given in ticks. I don't care if they are microseconds between incoming pulses. Before the timer overflow, all is well. Once it overflows, the count between pulses is about 1/4 or less what they should be even though PSC is the same. Consequently, the routine that looks at the timing thinks all pulses are fast after the overflow opposed to a scale of from 1 to 4 and all above 4 are treated the same way.
I'm looking at the RCC clock speed right now as I can't figure out why I am seeing 40 in the PSC register. I would have thought it should be 8 as I thought the RCC was running at 8Mhz.
But it no matter the accuracy of the count, it should be consistent and it isnt. After the overflow it is about 1/4th as fast.
What is the PSC in your TIM5?
Thanks
2018-11-30 8:28 PM
there is something hosed up that I don't understand. If I grab the TIM5 count, use HAL_Delay(10) for a 10ms delay, then grab the count again and subtract, no matter what I have in the PSC register I get the same approximate delta count of 789,354. It should be around 10,000. So I have something else wrong here that I don't understand. I mean, the setup code for TIM5 is pretty basic. I tried moving the PSC register from 39 to 7 and back to 3,200 with no change in the delta count.
I have to think about this now as it isn't working as expected. The overflow isn't set
2018-11-30 10:17 PM
well, I don't know why but adding below changed things and now it is working:
__HAL_RCC_TIM5_CLK_ENABLE();
TIM5->PSC=HAL_RCC_GetPCLK1Freq()/1000000-1;
TIM5->CR1=TIM_CR1_CEN | TIM_CR1_DIR;
I added TIM_CR1_DIR just as a test and for some reasons the TIM5 is now reporting closer to a microsecond. Before when I delayed like this:
mltime=TIM5->CNT;
HAL_Delay(10);
mctime=TIM5->CNT;
mstime=mltime-mctime;
mstime was being set to 798,000 give or take a few percent. Now it is down around 20,000 with the expectation that it would be around 10,000 for 10,000 microseconds.
I thought that TIM_CR1_DIR just set the countup or countdown direction but other than the direction something else must have changed. I had already changed the code to account for roll-over and I didn't change that code.
Anyway, unless someone can explain the reason why this is working I will just move on.
Thanks again Clive.
Jerry
2018-12-01 3:15 AM
The counter is upcounting unless CR1.DIR is set, so you should've calculated mstime = mctime - mltime.
JW