2016-10-05 3:39 PM
I am trying to set up TIM4 in Encoder Mode in Nucleo F767ZI. I used STM32CubeMX to set up the Timer. The TIM->CNT value oscillates between two values. On checking further, I found the DIR bit to be oscillating between 0 and 1. If I read the values of both the channels and do an external counting, it works fine. I am reading both edges on both the channels.
2016-10-06 1:09 PM
This is the TIM4 Init code as generated by Cube:
/* TIM4 init function */
static void MX_TIM4_Init(void)
{
TIM_Encoder_InitTypeDef sConfig;
TIM_MasterConfigTypeDef sMasterConfig;
htim4.Instance = TIM4;
htim4.Init.Prescaler = 0;
htim4.Init.CounterMode = TIM_COUNTERMODE_UP;
htim4.Init.Period = 0xffff;
htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
sConfig.IC1Polarity = TIM_ICPOLARITY_BOTHEDGE;
sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
sConfig.IC1Filter = 0;
sConfig.IC2Polarity = TIM_ICPOLARITY_BOTHEDGE;
sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
sConfig.IC2Filter = 0;
if (HAL_TIM_Encoder_Init(&htim4, &sConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
And I'm using
HAL_TIM_IC_CaptureCallback
to get the interrupts and calculate externally. At the same time I am comparing it to the TIM4->CNT value which doesn't seem to count up or down consistently.
2016-10-06 10:45 PM
I was working on something just like this just last night, but for a 407.
Try watching this:https://www.youtube.com/watch?v=GoRYhhdVR3MIgnore what he is saying, unless you understand Russian, but he shows all of the steps to do encoders using Cube.Andrei from The Great White North2016-10-07 1:28 AM
HiNeo,
I think you missed to add the start of Timer Encoder interface by adding the following (as example):/* Start the encoder interface */
HAL_TIM_Encoder_Start(&Encoder_Handle, TIM_CHANNEL_ALL);
Unfortunaly, the STM32CubeF7 does not contains an encoder example. You would take a look to another STM32Cube package like
which has the example ''TIM_Encoder''at this path: STM32Cube_FW_F4_V1.0\Projects\STM324xG_EVAL\Examples\TIM\TIM_Encoder
I will submit a request to add such example in the STM32CubeF7 package.
-Hannibal-
2016-10-07 5:20 AM
Hannibal,
I am starting the encoder using HAL_TIM_Encoder_Start(). I just posted the Timer initialization part that the Cube generated. The TIM4->CNT value changes, but it keeps going up and down, and so does the DIR bit. I am not sure why it is doing that, when the motor is consistently running in only one direction.Thanks.2016-10-07 6:54 AM
Hi Neo,
So try to play on ICpolarity, put one edge (up or down).-Hannibal-2016-10-07 7:44 AM
Thanks Hannibal!
It seems to be counting properly now.But I am wondering why is it so? Why can't it count properly when the ICPolarity is set to Both Edges?2016-10-07 8:43 AM
Hi Neo,
The both Edge Sensitive case is dedicated for another different encoding type .-Hannibal-