2024-09-15 02:41 PM
Hi,
as you can see from the screenshot below I have TIM2 clock source set to disable but the PWM is still running as configured and generates PWM. And it has been like that for the entire project for a while so I just noticed.
Does the time start function automatically select the source to some default like the Internal clock? Or is that Clock source referring to something else? Just asking because I want to make sure the code is running correctly for the right configuration not because of some other settings that somehow override these.
Thank you