TIM1_BKIN noise immunity problem
Hello,
I am using STM32VLDISCOVERY board. We have configured TIM1 in PWM mode with break feature enabled. But the BKIN input seems really sensitive and catches noise from the system resulting in a trip. Is there any data that says how much voltage on TIM1_BKIN pin (configured active low) will result in a fault detection ? Or is it the same ViL level as any other GPIO ?
Currently we have the pin configured as input_floating and externally pulled up to Vcc. We suspect that this external trace connectin BKIN and Vcc can catch up noise. If I configure the pin as internal pullup, will it still function as TIM1_BKIN ?
Thanks