2013-10-04 11:36 PM
I'm an absolutely beginner in microcontrollers.
I want to create a PWM signal wave signal to drive main power switch at 100Khz TIM1CH1&TIM1CH1N of STM32F103VC. I change duty (CCR1_Val) but the duty stay same at 50%. Can anybody tell me what I'm doing wrong? Thank You Photo to Attachments vu16 CCR1_Val = 90 ; TIM_DeInit(TIM1); /* Time Base configuration */ TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 360 - 1 ; // 72 MHz / 360 = 200 kHz TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1,&TIM_TimeBaseStructure); /* Channel 1, 2,3 and 4 Configuration in PWM mode */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle ; TIM_OCMode_PWM1 TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCNIdleState_Set; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; // 25% TIM_OC1Init(TIM1,&TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable); /* TIM1 counter enable */ TIM_Cmd(TIM1,ENABLE); /* Main Output Enable */ TIM_CtrlPWMOutputs(TIM1,ENABLE);2013-10-07 12:03 PM
Thank You very much but I have only TIM1CH1 pin free
I tried
to set TIM8 ( pin CH1 & CH2 free) (photo pin) but error comp. main.c(357): error: #20: identifier ''TIM1_UP_TIM10_IRQn'' is undefined ________________ Attachments : pin.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0dj&d=%2Fa%2F0X0000000bbm%2FmgyuHEhwGLe.R2F8scOCvx0Rj8bUP_oPj9X0KrcIEgg&asPdf=false2013-10-07 2:03 PM
The code was for an F4 rather than an F1 part, you will likely need to use a different interrupt designator, like TIM1_UP_IRQn, or TIM4_IRQn, etc, as appropriate, see stm32f10x.h and startup_stm32f10x.s
2013-10-08 12:16 AM
> One might suppose, but I've never had much joy with the dead-time settings, so an example doing this would be welcome.
Do you mean ''I tried but it did not work as I expected'', or ''I never had an opportunity/reason to try''? I don't have the reason, but as this is what one would expect as a driving waveform for a bridge, I'd be very surprised if ST wouldn't pay attention to its working. I'd even expect an example to exist somewhere. STM32F10x_StdPeriph_Lib_V3.4.0\Project\STM32F10x_StdPeriph_Examples\TIM\ComplementarySignals\ appears to be such, but as I said, so far I haven't had the reason to go there. JW2013-10-08 3:39 AM
Not problem JW,
thanks anyway
for help intentionwhen
you have a question
,
any ideas
welcome
to evaluate
or
test
2013-10-08 8:05 AM
Do you mean ''I tried but it did not work as I expected'', or ''I never had an opportunity/reason to try''?
Mostly the former, I have experimented with the timers, and tried to digest the documentation/diagrams. The timers only have a singular timing value, and I'm really not sure that I can combine say channel 1&2 and 3&4 to express a start/stop comparison with respect to the time base. I have experimented with dead-time settings, and had more frustration than success.Looking at the motor/pwm, multiple interrupt handlers for TIM1, I've concluded that they expect a much more dynamic interaction with the TIM parameters, rather that being able to set the hardware up once to perform some simple function generation automatically.2014-04-27 10:27 AM