TIM flags automatically set when TIM enabled
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-19 7:16 AM
Posted on June 19, 2013 at 16:16
The configuration for TIM3 is as follows, void TIM3_config(void) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructTIM3; NVIC_InitTypeDef NVIC_Init_TIM3 = {TIM3_IRQn, 2, 1, ENABLE}; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); TIM_TimeBaseStructTIM3.TIM_Period = 0x75A0; TIM_TimeBaseStructTIM3.TIM_Prescaler = 1; TIM_TimeBaseStructTIM3.TIM_ClockDivision = TIM_CKD_DIV4; TIM_TimeBaseStructTIM3.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructTIM3); /* TIM IT enable */ // TIM_ClearFlag(TIM3, TIM_FLAG_Update); NVIC_Init(&NVIC_Init_TIM3); TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE); } If you have any ideas where I should start looking for the problem, it'll be very helpful to progress in my work. #me-too
Hello,
I am facing a problem with the timers I am using in STM32f100 MCU. I have configured different timers to operate during the execution of the code, but somehow, all the flags related to Capture/compare or Update in the SR are set as soonas I enable the timer. As I read in the datasheet, they are all set in the hardware, and even if I clear them manually in debug mode, they are set again immidiately. My configuration for TIM3, for example, does not need any CC functionality, though i do use it in other timers. But considering that I need TIM3 only for generating a time base, I still dont understand why should the CC flags in SR be set. Below is the snapshot where I enable the TIM3 and the flags are set.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-19 7:16 AM
Posted on January 19, 2014 at 16:16
Hi,
I see the same ''strange'' automatic setting of TIM3->SR to 0x1F even after clearing IT flags.I tried many things but I don't find the solution.Is TIM_OCIdleState involved ?Anyway, I always see those flags rising, locking me into the IRQ Handler.Do you managed fixing it ?Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-19 7:59 AM
Posted on January 19, 2014 at 16:59
I'm not sure them being asserted is quite the same as them generating an interrupt, as that is masked by the enable bits.
If you look at them in a debugger, the machine is not running in real-time. Something interrupting a few 100 times a second is not practical for a human to process. If the CPU is constantly in the interrupt routine one should perhaps look at the prescaler/period values, and if they are impractically frequent. Perhaps showing the code that causes the issue would enable a better analysis?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..