cancel
Showing results for 
Search instead for 
Did you mean: 

There is an error when i debug my code in the stm23CubeIDE.

KP.3
Associate II

When I go to debug, there is an error saying some source file isnt found (__lib_init) or something like this. I dont remember the name exactly. Then it gives me an option to go to preferences. Also, the debug doesnt run properly, my peripheral registers arent changing value and Im not able to step into or step over or even resume although Im clicking the button. Please help me with this!!! What can I do (like add the required source file) and where can I find this file?

1 REPLY 1
TDK
Guru

How did you generate your project?

Add a screenshot of the exact error message.

If you feel a post has answered your question, please click "Accept as Solution".