cancel
Showing results for 
Search instead for 
Did you mean: 

The STM32F303RBT6 ADC2_IN3 data is abnormal when the pin PC4 set high.

lYong.1
Associate

The STM32F303RBT6 ADC2_IN3(PIN PA6) is connect to GND .When the pin PC4 set high,the ADC_IN3 read a abnormal data 0x70. When the pin PC4 set low,the ADC_IN3 read a normal data 0x00.

Which the PC4 set high,is affect theADC2_IN3 sample .

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

How exactly is PC4 set in GPIO?

> When the pin PC4 set high

Internally, i.e. setting PC4 to GPIO Out; or externally?

Doesn't the voltage on PC4 exceed VDDA?

JW