cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303RCT6 ADC读�?�异常

lYong.1
Associate

您好:

  我使用STM32F303RBT6的ADC2_IN3时,�?�现�?��?将PC4脚输出高电平时,ADC2_IN3采样的数�?�就会有异常。

   譬如ADC2_IN3脚接GND,PC4输出高电平,ADC采样�?�回的值为0x70;而将PC4输出低电平�?�,ADC采样就正常为0了。

   请问这是什么问题?

谢谢�?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @lYong.1​ ,

Commonly used languages in this community is English. Could you please translate your post?

Thanks,

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.