User Activity

The STM32F303RBT6 ADC2_IN3(PIN PA6) is connect to GND .When the pin PC4 set high,the ADC_IN3 read a abnormal data 0x70. When the pin PC4 set low,the ADC_IN3 read a normal data 0x00. Which the PC4 set high,is affect theADC2_IN3 sa...
您好:   我使用STM32F303RBT6的ADC2_IN3时,�?�现�?��?将PC4脚输出高电平时,ADC2_IN3采样的数�?�就会有异常。   譬如ADC2_IN3脚接GND,PC4输出高电平,ADC采样�?�回的值为0x70;而将PC4输出低电平�?�,ADC采样就正常为0了。   请问这是什么问题?谢谢�?