2018-08-08 8:56 AM
The *.stldr file generated by MX25LM51245G_STM32L4R9I-DISCO (@ ST-LINK Utility 4.2.0.0) can't work for STM32L4R9I-DISCO device.
Step1. According to the readme.txt in the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\MX25LM51245G_STM32L4R9I-DISCO", The detail is as follows:
@par Example Description
This an example of an external loader of MX25LM51245G flash memory for STM32L4R9I-DISCO.
This loader can be used with STM32 ST-LINK Utility and STM32CubeProgrammer.
@par Hardware and Software environment
- This example runs on STM32L4R9xx devices.
- This example has been tested with STMicroelectronics STM32L4R9I-Discovery
boards and can be easily tailored to any other supported device
and development board.
@par How to use it ?
- Place the folder "MX25LM51245G_STM32L4R9I-DISCO" under the following path inside the STM32L4 Cube firmware package "STM32Cube_FW_L4_Vx.y.z" folder:
STM32Cube_FW_L4_Vx.y.z\Projects\STM32L4R9I_DISCO\Examples\OSPI
- Open your preferred toolchain
- Rebuild all files and load your image into target memory
- After build, the loader should be displayed in the external loaders window, ready-to-use.
Step2. Add Existing project of MX25LM51245G_STM32L4R9I-DISCO by using the EWARM 8.22.1,then rebuild all files.So the
*.out file will be generated, then rename to *.stldr and copy to the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\"
IAR Configuration
Step3. When downloading MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex through ST-Link Utility 4.2.0.0,the error is as following:
23:49:29 : ST-LINK SN : 0678FF504955857567011028
23:49:29 : ST-LINK Firmware version : V2J29M18
23:49:29 : Connected via SWD.
23:49:29 : SWD Frequency = 4,0 MHz.
23:49:29 : Connection mode : Connect Under Reset.
23:49:29 : Debug in Low Power mode enabled.
23:49:29 : Device ID:0x470
23:49:29 : Device flash Size : 2MBytes
23:49:29 : Device family :STM32L4Rx
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] opened successfully.
Address Ranges [0x08000000 0x080001BC] [0x08006000 0x08006F48] [0x08007000 0x0803B303] [0x90000000 0x9022C30A]
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] checksum : 0x0F9EA60A
23:52:26 : Timeout during flash programming
23:52:26 : Error occured during erase operation!
Best Regards,
2018-08-08 9:07 AM
2018-08-08 9:10 AM
The ST-LINK Utilities external loader functionality is broken and the tool has been deprecated. Use the STM32Cube Programmer https://www.st.com/en/development-tools/stm32cubeprog.html
Support for external loaders is available on a contract basis.
2018-08-08 11:11 AM
The Cube Programmer uses the same External Loader structure/mechanics as the ST-LINK Utilities, but works properly.
They have abandoned support for the utilities, and I spent many fruitless hours trying to get HAL-QSPI to work on the F746-DISCO with the 4.2.0 release with errors/failures similar to those described here, the code I built ran properly with the Cube Programmer.
One quirk with the Cube Programmer is that the STLDR must have the exact same naming as in the machine readable header.
2018-08-08 4:19 PM
@ Clive Two.Zero
Thanks for your response.
The Cube Programmer can NOT work properly when downloading the *.hex by using the MX25LM51245G_STM32L4R9I-DISCO-OSPI.stldr(size : 148KB ) that it is generated by the source code of MX25LM51245G_STM32L4R9I-DISCO.But The Cube Programmer can work properly when downloading the *.hex by using the default MX25LM51245G_STM32L4R9I-DISCO.stldr (size: 156KB)@ "C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader".
Therefore,the issue is nothing to do with the download TOOL( Cube Programmer OR ST-Link Utility ), the source code or compile configuration is not good.
Best Regards,
2018-08-08 9:08 PM
I built this using my understanding of the process, with Keil uV5
2018-08-10 4:41 AM
2018-08-10 4:52 AM
With the one you created, or the one I attached above?
2018-08-10 6:39 AM
the one you attached ( 27KB ).
2018-08-10 7:01 AM
Ok, well fixing that is going to take some more work, likely going to run to several hundred dollars to resolve.