cancel
Showing results for 
Search instead for 
Did you mean: 

The output signals at the maximum frequency.

scolonel
Associate
Posted on December 21, 2011 at 12:45

How can I synchronize the timer output with a maximum frequency PLL,

ie 168 MHz.  In my example I set the timer to slow generate an interrupt,

which run fast timer for generating a single pulse duration of 6 ns,

but I have a jitter of 10 ns.

Example my codes:

1)

  /* Time base configuration TIM9 (fast)*/

  TIM_TimeBaseStructure.TIM_Period = 100;

  TIM_TimeBaseStructure.TIM_Prescaler = 0; // max freq. (168 MHz)

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 

  TIM_TimeBaseInit(TIM9, &TIM_TimeBaseStructure);

 

  /* TIM9 PWM2 Mode configuration: Channel1 */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 100;//get pulse ~6ns

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

 

  TIM_OC1Init(TIM9, &TIM_OCInitStructure);

 

  /* One Pulse Mode selection */

  TIM_SelectOnePulseMode(TIM9, TIM_OPMode_Single);

 

  /* Time base configuration TIM3 (slow) */

 

  TIM_TimeBaseStructure.TIM_Period = 1000;

  TIM_TimeBaseStructure.TIM_Prescaler = 8;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 

  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

 

  /* PWM1 Mode configuration: Channel4 */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0; // pulse for control

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

 

  TIM_OC4Init(TIM3, &TIM_OCInitStructure);

 

  //TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);

 

  TIM_ARRPreloadConfig(TIM3, ENABLE);

  /* TIM Interrupts enable */

  TIM_ITConfig(TIM3, TIM_IT_CC4 , ENABLE);

 

  /* TIM3 enable counter */

  TIM_Cmd(TIM3, ENABLE);

 

 2) config output pins

   /* TIM3 clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

    /* Enable peripheral clocks */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOE, ENABLE);

  /* TIM9 clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM9, ENABLE);

  /* TIM3_CH4 pin (PC.09) configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

 

  /* TIM9_CH1 pin (PE.05) configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOE, &GPIO_InitStructure);

 

3) interrupt config

  /* Enable the TIM3 gloabal Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

 

4) interrupt routine

void TIM3_IRQHandler(void)

{

  if (TIM3->SR & TIM_IT_CC4) //

  {

    /* Clear the IT pending Bit */

    TIM3->SR &= ~TIM_IT_CC4;

    TIM9->CR1 |= TIM_CR1_CEN; // start new pulse

  }

}

 

TIM9_CH1 (PE.05) output should be synchronized with TIM3_CH4 (PC.09) oputput, but it don't.

How to fix this trouble?

#stm32f4-discovery
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on December 21, 2011 at 17:39

The values for Prescale and Period take the form (N - 1)

For 1000 cycles, use 999

Pulse of 0 is always OFF, 1000 is always ON

Period = 100 - 1; // 100 cycles

Pulse = 99; // Low for a single tick, High for 99 (out of 100)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
scolonel
Associate
Posted on December 21, 2011 at 18:09

Thanks! B

ut

I installed the

other

pulse durations

, the jitter

is still

present.

Posted on December 21, 2011 at 20:10

If it is jitter, then I'd start by using clock sharing a common divider source (ie APB2) and the same prescaler.

A jitter of ~6ns suggests its falling on either side of an odd divider (asymmetrical duty cycle)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..