2022-09-02 12:21 AM
Hello,
I am working on project which contains reconfiguration of 16 regular channels ADC after end conversion sequence.
Therefore, the registers ADC_SQR1, ADC_SQR2, ADC_SQR3, ADC_SQR4 and ADC_SMPR1, ADC_SMPR2 should be updated at the end of the sequence each time.
This action takes some time and also CPU load.
Is there a documentation with recommendation or examples?
Can I use DMA for reconfiguration of ADC registers?
2022-09-04 12:29 AM
shure, try DMA