2018-04-02 1:37 PM
Hi guys:
I'm new here and just installed stm32cubemx 4.25 eclipse-plug-in.But when I started the eclipse , the plug-in's updater is automatically started and had always been 'checking' status.Now I can't do anything because 'the updater is already in use and checking server'.Does anyone know how can I stop the updater and install the stm32cubef4 packge myself.It would be better that I can stop the updater for good,since the network has always been problems for me.Many thanks.
2018-04-25 3:17 AM
Hi Guangrong,
To avoid automatic updates, I advise you to follow this simple steps:
1) Click on ?Updater Settings?:
2) Then, you have to choose ?Manual check? for ? check and Update Settings? and ?No Auto-Refresh at application start? for ?Data Auto-Refresh?:
3) Finally, you should restart eclipse to validate your modification:
Hoping it helps you, please let me know if it works for you.
In case of fail, please let me know:
If you are connecting via proxy or not
Your eclipse version
Additionally, it will be more helpful if you can send me your log file (
C:\Users\xxxxx\.stm32cubemx\STM32CubeMX.log) Please do not hesitate to contact me for further details.Best Regards,
Mohamed.
2018-04-25 6:16 AM
Hi Mohamed,
My english is not so good ,so if there is some phrasing mistakes,please forgive me.
I just solve my problem by reintalling my jre program.
I also use java for my work so I update my java to jre10 and find out that cubemx plug in is not work well with that edition,so I have to repalce it with jre1.8.0_161 and currently it works.
Thank you very much for your help.
Best Regards,
guangrong.