cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to build example projects NUCLEO-WB05KZ

utelettronico2
Associate II

STM32CubeIDE

Version: 1.12.1
Build: 16088_20230420_1057 (UTC)

I am trying to use one of the examples from the STM32Cube_FW_WB0_V1.1.0 package, but I am unable to build any of them.

After importing the project into STM32CubeIDE (I have tried BLE_Beacon and BLE_Power_Consumption), I attempt to build it, but I get the error shown in the image.

Cattura.PNG

At this point, I have to force close CubeIDE from the Task Manager because the program gets stuck with hundreds of error windows popping up.

I'm obviously missing a step, but I can't figure out which one. Has anyone encountered this issue before?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @utelettronico2 

The STM32CubeWB0 has been supported on the V1.16.0 of the STM32CubeIDE. So, could you please try to use the last version of the STM32CubeIDE (V1.18.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Souhaib MAZHOUD
ST Employee

Hello @utelettronico2 

The CubeIDE-1.12.1 does not support WB0 series, please upgrade your CubeIDE to the latest version.

BR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Hello @utelettronico2 

The STM32CubeWB0 has been supported on the V1.16.0 of the STM32CubeIDE. So, could you please try to use the last version of the STM32CubeIDE (V1.18.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.